How to fix error [Failed to connect to Excel events] occurs while Edit Using Spreadsheet in Drafting Application.

2021-10-06T23:28:01Z

Summary


Details

How to fix error [Failed to connect to Excel events] occurs while using  [Edit Using spreadsheet] option in Drafting Application.
error displayed.


Solution

Solution 1.
==========

1.Close NX.

2. Go To .... NX..\INSTALL folder.

3. Run the "unregister_splm_files.bat" and "register_splm_files .bat" file as administrator or by command prompt as an administrator.

4.Restart NX.

It is working fine when we run "unregister_splm_files.bat" and "register_splm_files.bat".


 If still facing issue after running bat files. refer solution 2.


Solution 2.
===========

We need to delete the below-mentioned registries from "Registry Editor" to work without error.


-------------- 
Delete:
HKEY_CLASSES_ROOT:
-REG DELETE HKEY_CLASSES_ROOT\CLSID\{D99CD578-9510-4014-9161-F01778698159} /f
-REG DELETE HKEY_CLASSES_ROOT\WOW6432Node\CLSID\{D99CD578-9510-4014-9161-F01778698159} /f
HKEY_LOCAL_MACHINE for 32-bit Excel:
-REG DELETE HKEY_LOCAL_MACHINE\SOFTWARE\Classes\WOW6432Node\CLSID\{D99CD578-9510-4014-9161-F01778698159} /f
-REG DELETE HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Classes\CLSID\{D99CD578-9510-4014-9161-F01778698159} /f
HKEY_LOCAL_MACHINE for 64-bit Excel:
-REG DELETE HKEY_LOCAL_MACHINE\SOFTWARE\Classes\CLSID\{D99CD578-9510-4014-9161-F01778698159} /f
--------------- 





Notes and References

10074167 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: xp64
Product: NX
Application: DRAFTING
Version: V1953
Function: TABLES

Ref: 002-8553671

KB Article ID# PL8553671

Contents

SummaryDetails

Associated Components